Is DDR required for K-70 LCDC?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is DDR required for K-70 LCDC?

2,028件の閲覧回数
mehmetoksan
Contributor I

Hello friends,

I am working with MK70FN1M0VMJ12 UC. I don't use TWR-K70-RGB LCD module. I want to control a TFT with MK70FN1M0VMJ12k without an external chip (SSD1963 or ILI.....)  and I am using  "eGUI". I tried to export an image with "eGUI" (size : 800x600, bit depth: 24, format : jpg) 

 

const LWord Aeshnid-ovipositing-800x600_data[] // array size:480000, 1875KB

 

But SRAM and LCD-RAM are as follows.

 

#define __EXTERNAL_MRAM_ROM_BASE 0xA0000000
#define __EXTERNAL_MRAM_ROM_SIZE 0x00000000
#define __EXTERNAL_MRAM_RAM_BASE 0xA0000000
#define __EXTERNAL_MRAM_RAM_SIZE 0x00080000
#define __EXTERNAL_DDR2_RAM_BASE 0x70000000
#define __EXTERNAL_DDR2_RAM_SIZE 0x08000000
#define __EXTERNAL_LCD_BASE 0xA0010000
#define __EXTERNAL_LCD_SIZE 0x0001FFFF//127KB
#define __EXTERNAL_LCD_DC_BASE 0xA0000000

#define __INTERNAL_SRAM_BASE 0x1FFF0000
#define __INTERNAL_SRAM_SIZE 0x00020000//128KB

 

So, Do I have to use DDR for LCDC?  or  Can I compress this image via "eGUI"?

 

Best Regards

 

Mehmet Okşan

Original Attachment has been moved to: 800_600_jpg.h.zip

Original Attachment has been moved to: 800_600_jpg.c.zip

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,901件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

Yes, customer can place picture at Flexbus connected MRAM memory.

It need to initialize Flexbus module during the system initialization phase (sysinit() at <start.c> file).


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信