Internal Vref for adc on K28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal Vref for adc on K28

1,649件の閲覧回数
jasonlarson
Contributor II

I'm working with adc reading and trying to decide if I should use the internal our external Vref for my results. During my testing I see that the internal vref seems to give me more stable readings but I see a couple issues. If anyone can explain them or has run across them please fill me in

1) Even though the Reference manual says the internal vref is 1.2v after I did some measuring it appears to be at 1.4v not 1.2v is this possible? Where do I set this voltage? I see I can change it by 0.5mv with a register but the max deviation from 1.2v is 30mv using this reg so not sure why I see 1.4v as the reference.

2) For some reason the first time I make the adc reading using internal vref I see a much higher readings than all the following readings if done with in 200ms. i.e my first sample of 16 readings averaged value was 3228 but when I run it again right after getting the 16 bit average I see 2998 and this only changes by 1 or 2 no matter how many more samples I take. Sure I can just ignore the first sample but want to know what causes it. If I leave things the same and just switch to using external vref and I don't see this error on the first reading. 

0 件の賞賛
返信
1 返信

1,547件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jason,

First of all, from hardware perspective, you have to connect 100nF with +/-25% tolerance capacitor to the Vref_OUT pin if you use internal 1.2V voltage reference.

Anyway, I think it is out of the range that the Vref_out pin voltage is 1.4V, ,pls test it with a digital meter.

BR

Xiangjun Rong

0 件の賞賛
返信