Integrating NXP Safety Library into Codewarriors Project.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Integrating NXP Safety Library into Codewarriors Project.

跳至解决方案
3,686 次查看
taimurwajad123
Contributor III

Hi all,

I'm using kinetis K10 and Codewarriors IDE. I wants to use NXP safety library IEC 60730B. I got the downloaded the latest version of library, which also supports Cortex CM4, but unfortunately the library is only compiled for IAR compiler.

Is there any possibility or workaround, so that I can use the library in my codewarrior project?

BlackNightHui_Ma

Any help shall be highly appreciated.

Best Regards

Taimur

0 项奖励
回复
1 解答
3,457 次查看
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,458 次查看
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

0 项奖励
回复
3,457 次查看
taimurwajad123
Contributor III

Hi,

Thanks for the reply.

So there is no way I can use this library in my code warrior project?

Regards

Taimur

0 项奖励
回复
3,457 次查看
miduo
NXP Employee
NXP Employee

Hi, Taimur

At present, no.

0 项奖励
回复