Integrating NXP Safety Library into Codewarriors Project.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Integrating NXP Safety Library into Codewarriors Project.

Jump to solution
3,887 Views
taimurwajad123
Contributor III

Hi all,

I'm using kinetis K10 and Codewarriors IDE. I wants to use NXP safety library IEC 60730B. I got the downloaded the latest version of library, which also supports Cortex CM4, but unfortunately the library is only compiled for IAR compiler.

Is there any possibility or workaround, so that I can use the library in my codewarrior project?

BlackNight‌ Hui_Ma

Any help shall be highly appreciated.

Best Regards

Taimur

0 Kudos
Reply
1 Solution
3,658 Views
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

View solution in original post

0 Kudos
Reply
3 Replies
3,658 Views
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

0 Kudos
Reply
3,658 Views
taimurwajad123
Contributor III

Hi,

Thanks for the reply.

So there is no way I can use this library in my code warrior project?

Regards

Taimur

0 Kudos
Reply
3,658 Views
miduo
NXP Employee
NXP Employee

Hi, Taimur

At present, no.

0 Kudos
Reply