Integrating NXP Safety Library into Codewarriors Project.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Integrating NXP Safety Library into Codewarriors Project.

ソリューションへジャンプ
3,813件の閲覧回数
taimurwajad123
Contributor III

Hi all,

I'm using kinetis K10 and Codewarriors IDE. I wants to use NXP safety library IEC 60730B. I got the downloaded the latest version of library, which also supports Cortex CM4, but unfortunately the library is only compiled for IAR compiler.

Is there any possibility or workaround, so that I can use the library in my codewarrior project?

BlackNight‌ Hui_Ma

Any help shall be highly appreciated.

Best Regards

Taimur

0 件の賞賛
返信
1 解決策
3,584件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,585件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Well, I really understood your feeling. However, the library itself was made based on IAR, unfortunately there is not plan to migrate this library to other IDE, for example the CodeWarrior. I am so sorry for the inconvenience this had caused.

0 件の賞賛
返信
3,584件の閲覧回数
taimurwajad123
Contributor III

Hi,

Thanks for the reply.

So there is no way I can use this library in my code warrior project?

Regards

Taimur

0 件の賞賛
返信
3,584件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Taimur

At present, no.

0 件の賞賛
返信