Installing FRDM-K22F - Tera Term

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Installing FRDM-K22F - Tera Term

2,561 Views
xmksa
Contributor I

Im on Win10

1. Downloaded the SDK Package

2. Downloaded and installed IDE

3. Downloaded and installed the driver while board is connected to PC via USB

4. Downloaded and installed Tera Term

 

So now I configured the serial port "speed" to 115200 just like in the tutorial, but after I connect the board I see no "data" floating. The "title" isnt "COMXX:115200baud Tera Term VT" but just "COMXX Tera Term VT"

0 Kudos
Reply
2 Replies

2,538 Views
nxf58904
NXP Employee
NXP Employee

 

nxf58904_5-1610518901656.png

 

 

0 Kudos
Reply

2,538 Views
nxf58904
NXP Employee
NXP Employee

Hi,

Can I ask which uart you used ?

Can you post more code for details?

If you refer the examples, the communication will success.

nxf58904_0-1610518189875.png

nxf58904_1-1610518241114.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply