Installing FRDM-K22F - Tera Term

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Installing FRDM-K22F - Tera Term

2,566件の閲覧回数
xmksa
Contributor I

Im on Win10

1. Downloaded the SDK Package

2. Downloaded and installed IDE

3. Downloaded and installed the driver while board is connected to PC via USB

4. Downloaded and installed Tera Term

 

So now I configured the serial port "speed" to 115200 just like in the tutorial, but after I connect the board I see no "data" floating. The "title" isnt "COMXX:115200baud Tera Term VT" but just "COMXX Tera Term VT"

0 件の賞賛
返信
2 返答(返信)

2,543件の閲覧回数
nxf58904
NXP Employee
NXP Employee

 

nxf58904_5-1610518901656.png

 

 

0 件の賞賛
返信

2,543件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

Can I ask which uart you used ?

Can you post more code for details?

If you refer the examples, the communication will success.

nxf58904_0-1610518189875.png

nxf58904_1-1610518241114.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信