Input voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Input voltage

1,769 次查看
martindusek
Contributor V

Is it safe to connect undefined voltage level (e.g. 1.5 V for 3.3 V MCU) on input pin of Kinetis MCU?

0 项奖励
回复
2 回复数

1,596 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

Base on analog issue, I think it will not damage anything. But base on digital logic, it might cause incorrect operation.

Best Regards

Paul

0 项奖励
回复

1,596 次查看
bobpaddock
Senior Contributor IV

Safe in what sense? A 1.5V input won't damage the part.

It may cause higher power consumption.

0 项奖励
回复