Input voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Input voltage

1,771件の閲覧回数
martindusek
Contributor V

Is it safe to connect undefined voltage level (e.g. 1.5 V for 3.3 V MCU) on input pin of Kinetis MCU?

0 件の賞賛
返信
2 返答(返信)

1,598件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

Base on analog issue, I think it will not damage anything. But base on digital logic, it might cause incorrect operation.

Best Regards

Paul

0 件の賞賛
返信

1,598件の閲覧回数
bobpaddock
Senior Contributor IV

Safe in what sense? A 1.5V input won't damage the part.

It may cause higher power consumption.

0 件の賞賛
返信