Input voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input voltage

1,775 Views
martindusek
Contributor V

Is it safe to connect undefined voltage level (e.g. 1.5 V for 3.3 V MCU) on input pin of Kinetis MCU?

0 Kudos
Reply
2 Replies

1,602 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Martin

Base on analog issue, I think it will not damage anything. But base on digital logic, it might cause incorrect operation.

Best Regards

Paul

0 Kudos
Reply

1,602 Views
bobpaddock
Senior Contributor IV

Safe in what sense? A 1.5V input won't damage the part.

It may cause higher power consumption.

0 Kudos
Reply