Input capture filter on FlexTimer (KV4x)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Input capture filter on FlexTimer (KV4x)

1,441 次查看
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

 a question regarding FTM on Kinetis:

40.4.19 Input Capture Filter Control (FTMx_FILTER)

This register selects the filter value for the inputs of channels.

CHxFVAL

Channel x Input Filter

Selects the filter value for the channel input.

The filter is disabled when the value is zero.

There are 4 bits for the filter values. How is the "effect" of filtering per 1 LSB of those 4 bits?

Does it basically tell how long the input signal have to be minimum (measured in system clock cycles) to go through the filter?

br

Guenter

0 项奖励
回复
1 回复

1,111 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guenter,

For the chapter of FTM module, here the system clock means the Fast Peripheral clock. We can find it in 'Table 6-1. Module clocks' of KV4XP100M168RM.

Table 6-1. Module clocks.png

For detail about the Filter, please read the '40.5.4.1 Filter for Input Capture mode'.

40.5.4.1 Filter for Input Capture mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复