Input capture filter on FlexTimer (KV4x)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Input capture filter on FlexTimer (KV4x)

1,409件の閲覧回数
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

 a question regarding FTM on Kinetis:

40.4.19 Input Capture Filter Control (FTMx_FILTER)

This register selects the filter value for the inputs of channels.

CHxFVAL

Channel x Input Filter

Selects the filter value for the channel input.

The filter is disabled when the value is zero.

There are 4 bits for the filter values. How is the "effect" of filtering per 1 LSB of those 4 bits?

Does it basically tell how long the input signal have to be minimum (measured in system clock cycles) to go through the filter?

br

Guenter

ラベル(2)
0 件の賞賛
返信
1 返信

1,079件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Guenter,

For the chapter of FTM module, here the system clock means the Fast Peripheral clock. We can find it in 'Table 6-1. Module clocks' of KV4XP100M168RM.

Table 6-1. Module clocks.png

For detail about the Filter, please read the '40.5.4.1 Filter for Input Capture mode'.

40.5.4.1 Filter for Input Capture mode.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信