Input Reflected issues with the kw36

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Input Reflected issues with the kw36

3,341 Views
loic_guillaume_
Contributor I

Hello,

I'm using the kw36 build in CRC hardware feature and i'm having some problem with it.

I must use a predefined crc (Init / Poly / XorOut) to match the decoder we already got.

To match the decoder, I must enable the CRC_CFG->CRC_REF_IN register but I'm having an error every 2 frames (ish)

With a 16 bit CRC, it is always the first bit of the second byte whose at fault. 

Example : 

D3 91 D3 91 10 01 00 11 22 33 00 00 01 02 0B A4 00 00 05 7F C3 > My frame transmitted

 

D3 91 D3 91 -> Sync (4 Bytes)

 

10 -> Length (on 8 bits) = payload (14) + CRC (2)

 

01 00 11 22 33 00 00 01 02 0B A4 00 00 05 -> Payload

7F C3 -> CRC sent

 

Or the correct one is 7F 43

CRC configuration :

    // Enable the CRC as it is disabled by default after reset

    XCVR_MISC->CRCW_CFG |= XCVR_CTRL_CRCW_CFG_CRCW_EN(1);

 

    GENFSK->CRC_CFG &= (uint32_t) ~(uint32_t) (GENFSK_CRC_CFG_CRC_SZ_MASK

                    | GENFSK_CRC_CFG_CRC_START_BYTE_MASK

                    | GENFSK_CRC_CFG_CRC_REF_IN_MASK

                    | GENFSK_CRC_CFG_CRC_REF_OUT_MASK

                    | GENFSK_CRC_CFG_CRC_BYTE_ORD_MASK);

 

    GENFSK->CRC_CFG |= (uint32_t) (GENFSK_CRC_CFG_CRC_SZ(2) // CRC16

                    | GENFSK_CRC_CFG_CRC_START_BYTE(4) // Start after the sync

                    | GENFSK_CRC_CFG_CRC_REF_IN(1) // Input reflected

                    | GENFSK_CRC_CFG_CRC_REF_OUT(1) // Output reflected

                    | GENFSK_CRC_CFG_CRC_BYTE_ORD(0)); // LSB first

 

    // Left align CRC seed and Poly.

    GENFSK->CRC_INIT = 0x00001D0F<< (2 << 3);

    GENFSK->CRC_POLY = 0x00001021 << (2 << 3);

    GENFSK->CRC_XOR_OUT = 0x00000000 << (2 << 3);

 

    GENFSK->XCVR_CFG &= ~GENFSK_XCVR_CFG_SW_CRC_EN_MASK;

CRC Value :

INIT = 0x1D0F<< (2 << 3);

POLY = 0x1021 << (2 << 3);

XOR_OUT = 0x0000 << (2 << 3);

My online checker (the reference) : Sunshine's Homepage - Online CRC Calculator Javascript 

Config :

pastedImage_2.png

If you have an idea of how to fix this, i will be grateful.

Regards,

Loïc

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

3,195 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please download the MCUXpresso SDK of KW36, then refer the CRC example.

You will get the 7F 43 after modify show below:

crc example.png

If you don't want to use APIs of MCUXpresso SDK, then you can configure CRC registers according to the image.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,195 Views
loic_guillaume_
Contributor I

Hello Robin,

Thanks for the reply,

The thing is,  when I check the calculated crc, it is the correct one (0x7F43) :

pastedImage_1.png

But the one sent is not (0x7FC3). 

And I'm sure it comes from the "sender" and not my receiver because if I set the crc manually (crc software), i always get the correct one. 

So I don't know how to explain that.

I would like to know, where the alteration happen.

Also, as I said, the problem dissapear if I disable the Ref input.

Regards,

Loïc

0 Kudos
Reply

3,195 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for my last reply! I didn't have KW36 on my hands. The CRC module seems different between K64 and KW36. 

But I don't know why you configure Input reflected and Output reflected.

For your predefined crc (Init / Poly / XorOut) and online checker, it seems you don't need to reflect input and output.(I didn't reflect in my example too.)

pastedImage_2.png

Best Regards,

Robin

0 Kudos
Reply

3,195 Views
loic_guillaume_
Contributor I

The thing is, to send 7F43 as the crc I need to reflect the input and the output on the sender side. 

In my previous reply, both are enabled. If you don't, the Online Crc and the one sent is different. 

Best Regards,

Loïc

0 Kudos
Reply

3,195 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I need to consult this with AE team and will update this thread as soon as I have their feedback. 

Best Regards,

Robin

0 Kudos
Reply