Input Glitch Filter in KEA-128?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Input Glitch Filter in KEA-128?

1,791 次查看
vigneshbalaji
Senior Contributor I

Hi,

    I wan to know about input glitch filter of KEA-128.

1) I want to filter out switch debouncing, Can I use Input Glitch Filter for it?

2)what is the maximum and minimum range in ms upto which Glitch filter can filter out?

Please provide relavent screenshots for the above questions.

标记 (3)
2 回复数

1,585 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Yes. You can use Input Glitch Filter for it.

The glitch width threshold can be adjusted easily by setting PORT_IOFLT0[FLTDIVn] between 1~4096 BUSCLKs (or 1~128 LPOCLKs).

The frequency of LPOCLK is 1KHz.

The BUSCLK depend on how you configure it.

Input glitch filter setting.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,585 次查看
vigneshbalaji
Senior Contributor I

Hi Robin,

                Can you give me an example calculation for min and max range of filter time with BUSCLK 24 Mhz?

0 项奖励
回复