Information on PCC INUSE Field

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Information on PCC INUSE Field

330 Views
sean_dvorscak
Contributor III

Hello,

I am looking for more information on the INUSE bit in the PCC registers.

The field in the Reference Manual of the KE1, says the bit indicates whether or not the peripheral is being used.

I ran some code waiting to see if the INUSE bit would set for a peripheral that I know was being used, and it never set.

I then looked in the SDK for the KE1 processor in Clocks.h, and saw the description of CLOCK_IsEnabledByOtherCore. The description says it checks whether the clock is already enabled and configured by any other core, and it does this by checking if the INUSE bit is set.

So what is the INUSE bit really telling us? Is it being used by the Core that enabled it, or another core?

I am also confused on what it means by "Enabled and configured by another core"? I only have one Core in the Processor. Is this only for multi-core?

0 Kudos
Reply
1 Reply

288 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @sean_dvorscak ,

Thanks for your post. I have already understood your confusion. The description in the SDK is indeed strange. I have now contacted the NXP internal team to support us on this topic and I'm waiting for their feedback. I will keep you updated about any new relevant information.

BRs,

Celeste

0 Kudos
Reply