If the debugging port is disabled, the program cannot be written. How to solve this problem?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If the debugging port is disabled, the program cannot be written. How to solve this problem?

Jump to solution
3,938 Views
kabusiji
Contributor I

As shown in the figure:

Debug.PNG

May I ask that the Debug was closed through PE configuration last time, but it cannot be burned in now, is there any solution?

 

Labels (1)
0 Kudos
Reply
1 Solution
3,932 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer the answer in: How to burn the program in KEA8 if SWD is disabled in main.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
3,926 Views
ErichStyger
Specialist I

The easiest way is to use the P&E Multilnk (it can be a 'normal' one), with the PEMICRO Recovery utility, see https://mcuoneclipse.com/2021/05/20/recovering-cortex-m-microcontroller-with-a-power-glitch/ and https://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-lo...

For the above you need the PEMicro debug probe.

If you have a J-Link, then you can try the 'resurrect locked Kinetis device' in the MCUXpresso IDE, see

ErichStyger_0-1647257501702.png

There is a command line way too, see https://mcuoneclipse.com/2014/10/05/unlocking-and-erasing-flash-with-segger-j-link/

 

I hope this helps,

Erich

0 Kudos
Reply
3,913 Views
kabusiji
Contributor I

Thanks!

0 Kudos
Reply
3,932 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer the answer in: How to burn the program in KEA8 if SWD is disabled in main.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,917 Views
kabusiji
Contributor I

Thanks

0 Kudos
Reply