IFR Program Once Read Command With Debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IFR Program Once Read Command With Debugger

1,641 Views
guitardenver
Contributor IV


Is there any way to read the program once IFR region with a debugger? Can the debugger tell the flash module to execute the Read Program Once Command (Assuming the device is un-secure)? For security reasons, external access to this region is unacceptable in our application.

MCU: MK22FN512

Debugger: Any

Thanks,

0 Kudos
Reply
2 Replies

1,438 Views
guitardenver
Contributor IV

Partly answered my own question.

Even if the debugger could not read that region,

If security is a concern, someone could issue a mass erase command and put their own program on their to read the IFR region themselves. So we will not be doing this.

0 Kudos
Reply

1,438 Views
bobpaddock
Senior Contributor III

Some devices can disable the Mass Erase command.

Doing so may make a lot of 'Bricked' devices if things are not fully thought through...

0 Kudos
Reply