IEC 60730 RAM test backup area

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IEC 60730 RAM test backup area

ソリューションへジャンプ
4,672件の閲覧回数
MLapaj
Contributor II

Hi, 

I've got a question regarding RAM test functions from IEC60730 4.0 library for Cortex-M0+.

While using FS_CM0_RAM_AfterReset() and FS_CM0_RAM_Runtime() functions, can the tested memory area include the RAM test backup area or does the backup have to be excluded from tested addresses?

Let's suppose the tesed area is from 0x1FFFF000 to 0x20002FFF, which is the whole RAM area. Can the backup area overlap with tested area (e.g. can the backup area be placed at 0x1FFFF800 address, as long as it is reserved)?

0 件の賞賛
返信
1 解決策
4,594件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

I have received feedback on the matter.

The backup memory  should not be placed inside of tested SRAM memory range.

Our suggestion to test all the SRAM range is to create a least two test interfaces, where the backup memory (for the first instance) will be placed in the second instance memory range and vice versa.

Thank you for your patience.

Regards,

Diego

 

元の投稿で解決策を見る

6 返答(返信)
4,655件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

If the backup memory is inside the tested memory (ovelap),  the tests functions   probably  destroy the contents stored in the backup area for a certain block on a certain  in a iteration.  I will recommend to avoid overlapping.

Br,

Diego.

 

0 件の賞賛
返信
4,629件の閲覧回数
MLapaj
Contributor II

I don't mind the backup area contents being destroyed since it's reserved area anyway. What I am worried about is receiving false negative result of a test. Is there any chance of that happening? 

Or are there any other consequences to test area and backup area overlapping?

 

0 件の賞賛
返信
4,617件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj ,

 I will consult  internally  to validate my reply to your inquiry. Could you let me know  the MCU that you are plannig to use with the library?

Thank you,

Diego.

0 件の賞賛
返信
4,611件の閲覧回数
MLapaj
Contributor II

Hi @diego_charles

It's being used only on Kinetis KE06 at the time. 

0 件の賞賛
返信
4,595件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @MLapaj 

I have received feedback on the matter.

The backup memory  should not be placed inside of tested SRAM memory range.

Our suggestion to test all the SRAM range is to create a least two test interfaces, where the backup memory (for the first instance) will be placed in the second instance memory range and vice versa.

Thank you for your patience.

Regards,

Diego

 

4,589件の閲覧回数
MLapaj
Contributor II

I understand. Thank you for your help.

0 件の賞賛
返信