IAR K10 Flash config

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAR K10 Flash config

2,302件の閲覧回数
dianel_cheng
Contributor I

Hi

   As the attached picture ,  I use IAR to debug MK10DX256ZVLQ10,but  i find there don't have 256K flash config to choose.

  And my IAR version is 6.50.5.  looking forward your help, thanks

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,121件の閲覧回数
Monica
Senior Contributor III

Hello wuxichengxv,

was that suggestion helpful? Please don't forget to keep us posted :smileywink:

Best regards,

Monica

0 件の賞賛
返信

2,121件の閲覧回数
chris_brown
NXP Employee
NXP Employee

Hi,

I believe you should be using the FlashK60Dxxx64.board file.  IAR distinguishes the different parts by the amount of SRAM the part has, which is 1/4 the flash size of the part.

Hope this helps,

Chris

0 件の賞賛
返信