IAR K10 Flash config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IAR K10 Flash config

2,318 Views
dianel_cheng
Contributor I

Hi

   As the attached picture ,  I use IAR to debug MK10DX256ZVLQ10,but  i find there don't have 256K flash config to choose.

  And my IAR version is 6.50.5.  looking forward your help, thanks

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

2,137 Views
Monica
Senior Contributor III

Hello wuxichengxv,

was that suggestion helpful? Please don't forget to keep us posted :smileywink:

Best regards,

Monica

0 Kudos
Reply

2,137 Views
chris_brown
NXP Employee
NXP Employee

Hi,

I believe you should be using the FlashK60Dxxx64.board file.  IAR distinguishes the different parts by the amount of SRAM the part has, which is 1/4 the flash size of the part.

Hope this helps,

Chris

0 Kudos
Reply