IAR,Error[Li005]: no definition for "__VECTOR_RAM"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IAR,Error[Li005]: no definition for "__VECTOR_RAM"

4,803件の閲覧回数
710787859
Contributor I

I'm coding。IC is MKE02Z64 and IDE is IAR. There are three link errors and i can't deal with them. What should i do?

Error[Li005]: no definition for "__VECTOR_TABLE"

Error[Li005]: no definition for __VECTOR_RAM"
Error[Li005]: no definition for "__BOOT_STACK_ADDRESS"

0 件の賞賛
返信
4 返答(返信)

3,858件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi

Could you let me know your SDK version and IAR version?

If you are using SDK 2.4, then you need to upgrade your IAR to version 8.22.

Please check the release note for more details

pastedImage_1.png

Regards

Daniel

0 件の賞賛
返信

3,858件の閲覧回数
710787859
Contributor I

My IAR version is 8.22. I don't use SDK and just copy startup files from FRDM-KE02 to my new project.

I don't find the definition of "__VECTOR_TABLE","__VECTOR_RAM", "__BOOT_STACK_ADDRESS".

0 件の賞賛
返信

3,858件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Baode

Addresses for VECTOR_TABLE and VECTOR_RAM  and __BOOT_STACK_ADDRESS come from the linker file,  I would suggest you check your linker file.

Regards

Daniel

0 件の賞賛
返信

3,858件の閲覧回数
710787859
Contributor I

Hi Daniel,

I have checked my linker file. There is no problem. And I open the linker file and can't find the definitions. Is this a bug of IAR8.22? could you give me a KE02 project based on IAR8.22?

0 件の賞賛
返信