I2S Driver with demo example for FRDMK28 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2S Driver with demo example for FRDMK28 board

1,253件の閲覧回数
vinod_alibade
Contributor I

Hi,

Please provide I2S driver along with demo example for FRDMK28 board as early as possible.

Thanks

Rekha#

0 件の賞賛
返信
1 返信

1,168件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Vinod Alibade

As long as this frdm board doesn't have a codec onboard, there is no any example using the SAI module in the SDK package. But you can base your example on other MCU. frdm-k66f does have a codec (Dialog) and in the SDK software it includes an SAI example, I would recommend you to download the software from the page:

Welcome | MCUXpresso SDK Builder 

And check the example under "driver example", it should use the same APIs that are with the K28 MCU. Please check it and tell me if you have any question about it.

Best regards

Jorge Alcala

0 件の賞賛
返信