I2S Driver with demo example for FRDMK28 board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I2S Driver with demo example for FRDMK28 board

1,256 次查看
vinod_alibade
Contributor I

Hi,

Please provide I2S driver along with demo example for FRDMK28 board as early as possible.

Thanks

Rekha#

0 项奖励
回复
1 回复

1,171 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Vinod Alibade

As long as this frdm board doesn't have a codec onboard, there is no any example using the SAI module in the SDK package. But you can base your example on other MCU. frdm-k66f does have a codec (Dialog) and in the SDK software it includes an SAI example, I would recommend you to download the software from the page:

Welcome | MCUXpresso SDK Builder 

And check the example under "driver example", it should use the same APIs that are with the K28 MCU. Please check it and tell me if you have any question about it.

Best regards

Jorge Alcala

0 项奖励
回复