Hi
The K70 is the only Kinetis part with internal LCD controller.
However many LCDs contain a controller chip and can be easily interfaced to the FlexBus as alternative (many Kinetis parts have the FlexBus). I many cases such graphical LCDs can also be driven by simply 'bit-banging' the bus interface too.
Reference:
1. The TWR-LCD-RGB has a pure LCD in it and so can only be used together with the K70
2. The TWR-LCD module has a graphical LCD with in-built controller which can be used with many Kinetis parts via FlexBus
See also http://www.utasker.com/docs/uTasker/uTaskerLCD.PDF
and https://www.youtube.com/watch?v=AdtRyQ-2IrE
Regards
Mark
P.S. The SLCD controller is not of use with graphical LCDs. It controls just segment LCDs.
References:
- http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf
- https://www.youtube.com/watch?v=nm2DmZv1rj8