I can't share the pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I can't share the pins

2,034 Views
piergiacomi
Contributor II

I have a problem with Kinetis studio, I can't share the pins because the expert mode is not settable there are only basic and advanced.

I hope you can help me, thank you very much.

0 Kudos
Reply
6 Replies

1,825 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi GABRIELE VALLESI,

Right click the pin that you want to share, and then enable it.

Pin Sharing Enabled.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------

1,825 Views
piergiacomi
Contributor II

Hi Robin,

thanks a lot for the answer, but my problem is that the Pin Sharing is disabled

thank

GabrieleSenza titolo-3.jpg

0 Kudos
Reply

1,825 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Would you please tell me the part number of your MCU?
Please also show me which component of Processor Expert are used.

Best Regards,

Robin

1,825 Views
piergiacomi
Contributor II

Hi Robin,

I'm using MKE06Z128VLD4 and the component is module SPI (Kinetis/AsynchroMaster).

I use this module to send only the data to external DAC and I don't need the DIN pin.

Thank you very much for your help.

Best Regards

Gabriele

Senza titolo-3.jpg

0 Kudos
Reply

1,825 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Similar problems have been discovered before: Pin sharing not allowed between Capture and BitIO component (Kinetis KE06)

Taking into account the specificity of the PTB4 pin, would you please use other SPI pins?

SIM_SOPT0[NMIE].png

Best Regards,

Robin

0 Kudos
Reply

1,825 Views
piergiacomi
Contributor II

Hi Robin,

I need to use the PB4 pin for an output but it is blocked by the SPI for the DIN signal that I don't need and that I can't disable, can you help me?

thank you very much for your help

best regards

Gabriele

0 Kudos
Reply