I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical interface in RMII mode by keeping MII pins remain connected or

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I am using freescale K70 series microcontroller (part number MK70FN1M0VMJ12) I have interfaced Ethernet switch IC ( part number LAN9303i) in MII. Whether Can I use this physical interface in RMII mode by keeping MII pins remain connected or

816 Views
shivakumarlv
Contributor I

By  keeping  physical connection of MII interface can I use RMII mode.or I need to provide jumper settings.

0 Kudos
Reply
1 Reply

744 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I think that's Ok for customer to connects MII pins with Ethernet PHY, while customer just want to use RMII mode.

Customer could refer TWR-SER2 board, which is using DP83849I(two Ethernet PHY) provides MII and RMII connection.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply