HyperBus/QSPI Flash and RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HyperBus/QSPI Flash and RAM

4,258件の閲覧回数
a8Chcx
Contributor V

Hi,

I am using K66F and KV58F for our controller. I want to expand the flash and RAM on Flexbus or SPI of K66F and KV58F?

Can anyone tell if I can us Hyperbus/QSPI Flash and RAM? Is there any recommend way to expand Flash and RAM by using less IO pins?

Thanks,

Christie

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,333件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Christie,

Of course, you can use FlexBus to extend NOR flash and normal SRAM, as you said the connection needs more pins, it needs address bus, data bus and control bus.

The K66F and KV58F has spi module, but it is normal spi module instead of qspi or hyperbus, in other words, KV58 and K66 can not connect with qspi or hyperbus SRAM or flash.

We have Kinetis K8x, they have on-chip qspi module, which can connect with flash or SRAM with qspi interface.

Hope it can help you

BR

Xiangjun rong

0 件の賞賛
返信

3,333件の閲覧回数
a8Chcx
Contributor V

Hi Xiangjun,

Thank you.

Can I use SPI on K66F and KV58 to connect SPI flash? If yes, can you recommend any SPI/QSPI flash that can be used on K66F and KV58?

Thanks,

Christie

0 件の賞賛
返信

3,333件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Christie,

This is the spi flash link, you can select one.

https://www.mouser.com/Semiconductors/Integrated-Circuits-ICs/Memory-Storage/Flash-Memory/_/N-98xbh?... 

Hope it can help you

BR

Xiangjun rong

0 件の賞賛
返信