How to use the internal 1.2v reference for ADC on K60 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the internal 1.2v reference for ADC on K60 ?

Jump to solution
1,524 Views
danielchai
Senior Contributor I

Hi All,

I am using the MQX10.4 and MQX4.0.1.

I was trying to use the internal 1.2v reference for adc0.

I used ioctl(adc_dev0, ADC_IOCTL_SET_REFERENCE, ADC_REF_VREF), but when I check the register SC2 reference bits still shows 00.

I also tried to manually set the VREF_SC  and SC2 register.

VREF_SC |= 0xA0;

ADC0_BASE_PTR ->SC2 |= 0x01;

but the reading result still based on VREFH and VREFL not based on internal 1.2v.

Any suggestion about this?

Thanks.

0 Kudos
Reply
1 Solution
1,235 Views
danielchai
Senior Contributor I

The ADC_REF_VREF does not work. But change it to ASC_REF_VALT, IT WORKS.

View solution in original post

0 Kudos
Reply
2 Replies
1,236 Views
danielchai
Senior Contributor I

The ADC_REF_VREF does not work. But change it to ASC_REF_VALT, IT WORKS.

0 Kudos
Reply
1,235 Views
DavidS
NXP Employee
NXP Employee

Hi Daniel,

Sorry for trouble but very glad you resolved it.  Good debugging on your part.

There is also Freescale AN4568 that uses internal voltage reference for Kinetis K series that might help others.

Regards,

David

0 Kudos
Reply