How to use peg lite?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use peg lite?

2,329 Views
francescogerard
Contributor I

i have a k70 tower with an lcd module and serial module. That i want is load a demo gui in the tower.i have download egui official demo from the nxp site but i dont have idea how to load this demo in the tower...Which tool have i need?there is a guide that explain the procedure to do? is possible use peg lite without mqx and code warrior?thanks all

0 Kudos
Reply
3 Replies

1,983 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Francesco Gerardi,

    About the egui guide, please refer to this post:

Getting started with the eGUI (a.k.a. D4D)

    This document is also based on the TWR-K70F120M board.

    You can use the peg lite without mqx and codewarrior, but we don't have the according sample code now.

Wish it helps you!

If you still have question, please contact me!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,983 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

PEG Lite includes examples for K70.

http://www.nxp.com/products/software-and-tools/run-time-software/peg-graphics-software/peg-lite-runt...

You can request a Lite license writing email to: [email protected]

Luis

0 Kudos
Reply

1,983 Views
francescogerard
Contributor I

Hi Jingjing Zhou.

Thanks for your answer.

My problem is that I don’t want use codewarrior, mqx or iar but if possible I should use kinetis design studio.

I have two question for you :smileyhappy:

1) can I load a new project from kinetics on the tower with the usb ???

2) if exsist a demo peg lite, can I load this demo from the kinetics to the tower?or in general, can I load some gui demo on the tower from kinetics trough the usb???

thanks

Da: kerryzhou

Inviato: venerdì, 4. marzo 2016 04:00

A: Francesco Gerardi <[email protected]>

Oggetto: Re: - How to use peg lite?

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

How to use peg lite?

reply from Jingjing Zhou <https://community.freescale.com/people/kerryzhou?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion <https://community.freescale.com/message/621327?et=watches.email.thread#621327>

0 Kudos
Reply