How to use RTS and CTS for UART communication?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use RTS and CTS for UART communication?

2,515件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hello

I am using UART for communication between 2uc I was wondering to use RTS and CTS as through this I can reduce the data loss but I was unable to do it so I wanted the hardware and code wise explanation for this So I wanted to know If there is any application note on this? Also I was wondering can I use these pins for RS-422 communication  using multiple uc interacting at same time ? But obviously 1 master and multiple slaves.

Thanks & Regards

Amit Kumar

タグ(5)
0 件の賞賛
返信
1 返信

1,680件の閲覧回数
Amit_Kumar1
Senior Contributor II

Hi

in Serial_LDD component of processor expert, I have enabled the RTS, CTS but I couldn't find its function in the method i.e when i checked in help for Serial_LDD there was functions to enable RTS and CTS but after selecting these options in the component properties, it still didn't came in methods. I wanted to know how to use these in my program.

pastedImage_2.png

pastedImage_3.png

from help ,

pastedImage_4.png

What is this peripheral support feature?

Thanks and Regards

Amit Kumar

0 件の賞賛
返信