which Kinetis cuod support I2C master spec :Sm/Fm/Fm /Hs modes (100/400/1000/3400 kHz)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

which Kinetis cuod support I2C master spec :Sm/Fm/Fm /Hs modes (100/400/1000/3400 kHz)

1,203 Views
r58737
NXP Employee
NXP Employee

Hello ,

I would like to know is there is a Kinetis serie that can handle such I2C spec:

Sm/Fm/Fm /Hs modes (100/400/1000/3400 kHz)

Thanks

Rgds

Philippe

0 Kudos
2 Replies

1,018 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Philippe,

Kinetis’s I2C is targeted for compliance to I2C specifications for standard (100kHz) and fast mode (400kHz).

The maximum communication length and the number of devices that can be connected are limited by a maximum bus capacitance of 400 pF.

Although Kinetis's I2C is capable of operating at higher baud rates, up to a maximum of (bus clock/20) with reduced bus loading, it does not have a special circuit to pull up the SCL and SDA lines to achieve high speed mode (up to 3.4MHz) compliance.

Wish it helps.

B.R.

Ma Hui

0 Kudos

1,018 Views
r58737
NXP Employee
NXP Employee

Thanks !

Rgds

Philippe

0 Kudos