Sorry for asking this basic question. I am very new to this area. My board is KL05Z.
From the reference manual, the duty cycle is determined by "CnV". so I simply added the following lines to LED_Blink.c (before the while loop).
However, this did not work. When I run this piece of code in the board, it throws me to HardFault_Handler.
TPM0_C0V = 1;
TPM0_C1V = 1;
TPM0_C2V = 1;
TPM0_C3V = 1;
TPM0_C4V = 1;
while(1)
{
Delay(200000);
LED1_TOGGLE;
Delay(200000);
LED2_TOGGLE;
Delay(200000);
LED3_TOGGLE;
}
What's the proper way of setting the duty cycles in PWM? I attached this piece of code in MKL05Z4.h, Hopefully it is easier for people with experience to look at.
Thanks a lot!
/** TPM - Peripheral register structure */
typedef struct TPM_MemMap {
uint32_t SC; /**< Status and Control, offset: 0x0 */
uint32_t CNT; /**< Counter, offset: 0x4 */
uint32_t MOD; /**< Modulo, offset: 0x8 */
struct { /* offset: 0xC, array step: 0x8 */
uint32_t CnSC; /**< Channel (n) Status and Control, array offset: 0xC, array step: 0x8 */
uint32_t CnV; /**< Channel (n) Value, array offset: 0x10, array step: 0x8 */
} CONTROLS[6];
uint8_t RESERVED_0[20];
uint32_t STATUS; /**< Capture and Compare Status, offset: 0x50 */
uint8_t RESERVED_1[48];
uint32_t CONF; /**< Configuration, offset: 0x84 */
} volatile *TPM_MemMapPtr;
/* TPM - Register accessors */
#define TPM_SC_REG(base) ((base)->SC)
#define TPM_CNT_REG(base) ((base)->CNT)
#define TPM_MOD_REG(base) ((base)->MOD)
#define TPM_CnSC_REG(base,index) ((base)->CONTROLS[index].CnSC)
#define TPM_CnV_REG(base,index) ((base)->CONTROLS[index].CnV)
#define TPM_STATUS_REG(base) ((base)->STATUS)
#define TPM_CONF_REG(base) ((base)->CONF)
/* TPM - Register instance definitions */
/* TPM0 */
#define TPM0_SC TPM_SC_REG(TPM0_BASE_PTR)
#define TPM0_CNT TPM_CNT_REG(TPM0_BASE_PTR)
#define TPM0_MOD TPM_MOD_REG(TPM0_BASE_PTR)
#define TPM0_C0SC TPM_CnSC_REG(TPM0_BASE_PTR,0)
#define TPM0_C0V TPM_CnV_REG(TPM0_BASE_PTR,0)
#define TPM0_C1SC TPM_CnSC_REG(TPM0_BASE_PTR,1)
#define TPM0_C1V TPM_CnV_REG(TPM0_BASE_PTR,1)
#define TPM0_C2SC TPM_CnSC_REG(TPM0_BASE_PTR,2)
#define TPM0_C2V TPM_CnV_REG(TPM0_BASE_PTR,2)
#define TPM0_C3SC TPM_CnSC_REG(TPM0_BASE_PTR,3)
#define TPM0_C3V TPM_CnV_REG(TPM0_BASE_PTR,3)
#define TPM0_C4SC TPM_CnSC_REG(TPM0_BASE_PTR,4)
#define TPM0_C4V TPM_CnV_REG(TPM0_BASE_PTR,4)
#define TPM0_C5SC TPM_CnSC_REG(TPM0_BASE_PTR,5)
#define TPM0_C5V TPM_CnV_REG(TPM0_BASE_PTR,5)
#define TPM0_STATUS TPM_STATUS_REG(TPM0_BASE_PTR)
#define TPM0_CONF TPM_CONF_REG(TPM0_BASE_PTR)
/* TPM1 */
#define TPM1_SC TPM_SC_REG(TPM1_BASE_PTR)
#define TPM1_CNT TPM_CNT_REG(TPM1_BASE_PTR)
#define TPM1_MOD TPM_MOD_REG(TPM1_BASE_PTR)
#define TPM1_C0SC TPM_CnSC_REG(TPM1_BASE_PTR,0)
#define TPM1_C0V TPM_CnV_REG(TPM1_BASE_PTR,0)
#define TPM1_C1SC TPM_CnSC_REG(TPM1_BASE_PTR,1)
#define TPM1_C1V TPM_CnV_REG(TPM1_BASE_PTR,1)
#define TPM1_STATUS TPM_STATUS_REG(TPM1_BASE_PTR)
#define TPM1_CONF TPM_CONF_REG(TPM1_BASE_PTR)
Solved! Go to Solution.
 
					
				
		
It "knows" how to write the code, If you know how to write the code, then no problem.
I recommend this because then you can look at the generated code and see how to do it.
I suppose I could post some code, but then I would deny you pleasure of learning.
BTW You are getting the hard fault because you did not set the clock gate in SIM_SCGC6.
 
					
				
		
Hi,
You need to configure TPM as PWM and select a channel in this case One of the RGB led.
In the attachments you can find the code for a short application using TMP0 to change duty in RED led (PTB4 TPM0_CH1) Compare this code with yours and see what every register does.
Hope this helps.
 
					
				
		
Hey Adrian,
Thanks for the help.
I read your code for TPM.
I am driving a relay by FET so GPIO output will be connected to FET.
The requirement is to have an ON/OFF button and when ON is pressed the Relay should be closed for 1 second and then opened for 9 seconds and repeat the loop 1000 times or until OFF is pressed.
I am wondering how your code will change and how the 'duty' will change?
Thanks
Victor
 
					
				
		
anybody who would like to help?
 
					
				
		
You need to properly set up the TPM.
Create another project and use PE to set up the TPM for PWM.
 
					
				
		
Hi Jim,
Thank you so much for your reply. I am a newbie so this might just be another ignorant question...
What does PE do that I can't do? My understanding is that I can just write code, build, program and the board would run. I imagine I can just add/edit code to set up the TPM, in my current code?
Thanks again.
 
					
				
		
It "knows" how to write the code, If you know how to write the code, then no problem.
I recommend this because then you can look at the generated code and see how to do it.
I suppose I could post some code, but then I would deny you pleasure of learning.
BTW You are getting the hard fault because you did not set the clock gate in SIM_SCGC6.
Hi Jim,
I want to make my led dim using tpm without using processor expert. Could you help me? i am new to kinetis world so i do not know where to start. BTW i'm using kl26z.
Thank You.
Regards,
Ken