How to trigger adc by pdb?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to trigger adc by pdb?

1,993件の閲覧回数
Alan_LIU
Contributor I

I use frdm-kv31f, the sdk version is 2.10, I want to implement pdb to trigger adc, the example of sdk is not clear.

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,973件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

Please refer: AN12374 PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors 
It may help you understand the relationship between FTM PDB ADC

Hardware timing and synchronization.png

AN12374SW

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,967件の閲覧回数
myke_predko
Senior Contributor III

@Robin_Shen 

Nice graphic - it's always useful if you can visually show what's happening in the system.  

0 件の賞賛
返信

1,984件の閲覧回数
myke_predko
Senior Contributor III

Hi @Alan_LIU 

Can you provide a bit more information?  What do you have working (ie PDB IRQ, ADC configure, ADC start conversion, ADC return conversion value)?  

Could you describe what you want to do?

0 件の賞賛
返信