How to trigger adc by pdb?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to trigger adc by pdb?

2,057 Views
Alan_LIU
Contributor I

I use frdm-kv31f, the sdk version is 2.10, I want to implement pdb to trigger adc, the example of sdk is not clear.

 

Labels (1)
0 Kudos
Reply
3 Replies

2,037 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

Please refer: AN12374 PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors 
It may help you understand the relationship between FTM PDB ADC

Hardware timing and synchronization.pngHardware timing and synchronization.png

AN12374SW

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,031 Views
myke_predko
Senior Contributor III

@Robin_Shen 

Nice graphic - it's always useful if you can visually show what's happening in the system.  

0 Kudos
Reply

2,048 Views
myke_predko
Senior Contributor III

Hi @Alan_LIU 

Can you provide a bit more information?  What do you have working (ie PDB IRQ, ADC configure, ADC start conversion, ADC return conversion value)?  

Could you describe what you want to do?

0 Kudos
Reply