How to trigger adc by pdb?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to trigger adc by pdb?

2,087件の閲覧回数
Alan_LIU
Contributor I

I use frdm-kv31f, the sdk version is 2.10, I want to implement pdb to trigger adc, the example of sdk is not clear.

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,067件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Alan,

Please refer: AN12374 PMSM Field-Oriented Control on FRDMKV31F with Hall and Encoder Sensors 
It may help you understand the relationship between FTM PDB ADC

Hardware timing and synchronization.pngHardware timing and synchronization.png

AN12374SW

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,061件の閲覧回数
myke_predko
Senior Contributor III

@Robin_Shen 

Nice graphic - it's always useful if you can visually show what's happening in the system.  

0 件の賞賛
返信

2,078件の閲覧回数
myke_predko
Senior Contributor III

Hi @Alan_LIU 

Can you provide a bit more information?  What do you have working (ie PDB IRQ, ADC configure, ADC start conversion, ADC return conversion value)?  

Could you describe what you want to do?

0 件の賞賛
返信