How to send LEFT and RIGTH channel data through I2S of KL26?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to send LEFT and RIGTH channel data through I2S of KL26?

1,553件の閲覧回数
2743294708
Contributor I

The KL26 MCU has only one Transmit Data Rigister(TDR). So how to  send LEFT and RIGTH channel data through I2S?

In my test, the data of left channel and right channel of KL26 is same, when wirte data to TDR.

pastedImage_1.png

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,463件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Customer can refer below picture to use SAI_TX_SYNC signal to select LEFT/RIGHT channel.

pastedImage_1.png

Customer can use I2Sx_TCR4[FSP] bit ( Frame Sync Polarity)  to set active level.

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信