How to program KL-MCUs by P&E usb multilink universal?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program KL-MCUs by P&E usb multilink universal?

ソリューションへジャンプ
9,110件の閲覧回数
w_x
Contributor II

Hi All:

I have one Usb Multilink Universal programmer which version is V1. There is no SWD support information on user's guide.

But I found that P&E have announced Usb Multilink Universal supporting for Kinetis L series MCUs.

How can I use my own Usb Multilink Universal to program KL-MCUs? Need to update the firmware of programmer?

Pls see the attached files.

THX!

-------------------------------------------------------------------------------------------------------------------

old.png

---------------------------------------------------------------------------------------------------------------------

new.png

ラベル(2)
0 件の賞賛
返信
1 解決策
8,021件の閲覧回数
BlackNight
NXP Employee
NXP Employee

P&E Universal Multilink does an update automatically as needed at the time of connect. Reasons for an update are

- updated (newer version) of the firmware available (e.g. you have V1 on the Multilink, but your debugger has >V1 available)

- switching Processor (e.g. from a ColdFire to a Kinetis): in that case a different firmware is needed on the Multilink, and it is downloaded to the Multilink automatically

Additionally P&E has a utility on their website to inspect the firmware version and to upgrade/downgrade the firmware.

Hope this clarifies it,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
8,021件の閲覧回数
marceli1
Contributor III

The most common mistake is wrong wiring to match pins between Multilink and PCB board. Therefore Reset pin is always low!

0 件の賞賛
返信
8,021件の閲覧回数
JimDon
Senior Contributor III

It does support SWD, I am using to program and debug the Freedom board, but I did have to solder in a .05" header.

Refer to a schematic of  similar Freescale reference board to see  to how to connect it on your prototype board.

0 件の賞賛
返信
8,021件の閲覧回数
w_x
Contributor II

Thanks, Jim.

Mostly what I care about is if there is need to update the firmware of Usb Multilink Universal?

It will be good news if we can use it without any change.

0 件の賞賛
返信
8,021件の閲覧回数
JimDon
Senior Contributor III

Well, if the firmware need to be updated, CW will do that the first time you connect. You will get a dialog say it is updating the firmware.

I think it did.

0 件の賞賛
返信
8,022件の閲覧回数
BlackNight
NXP Employee
NXP Employee

P&E Universal Multilink does an update automatically as needed at the time of connect. Reasons for an update are

- updated (newer version) of the firmware available (e.g. you have V1 on the Multilink, but your debugger has >V1 available)

- switching Processor (e.g. from a ColdFire to a Kinetis): in that case a different firmware is needed on the Multilink, and it is downloaded to the Multilink automatically

Additionally P&E has a utility on their website to inspect the firmware version and to upgrade/downgrade the firmware.

Hope this clarifies it,

Erich

0 件の賞賛
返信