How to know if configure line as bit ldd or gpio ldd

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to know if configure line as bit ldd or gpio ldd

1,145 Views
haroldvogel
Contributor II

I am working with a MKL36Z256VLL4 chip.  I need to configure a line to send a reset signal to external device.  How do I know if I should configure the line as a BIT_LDD or GPIO_LDD or something else.  The pin is PTB8 on the chip.

Tags (1)
0 Kudos
Reply
1 Reply

1,050 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Harold,

You can both of them. I think BitIO_LDD is simple .

About the detail  introduce about the components, please find from "General Info":

right lick the component ->  Help on component .

There also are Typical Usage.

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply