How to implement USB Mass storage class in MK60FN1M0VLQ12

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to implement USB Mass storage class in MK60FN1M0VLQ12

3,259 Views
rajkumar_yerraj
Contributor II

Hi,

I want to implement USB Mass storage class with MK60FN1M0VLQ12 controller. I want to configure it in Device Mode. Does it require an external USB Transceiver ?

Kindly provide me sample code if anything is available for it.

Thank you.

-Gangadhar

Labels (2)
0 Kudos
Reply
3 Replies

3,057 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

You can download our SDK from our MCUXpresso website. Once downloaded you can import the sdk examples.

pastedImage_1.png

The K60 already has the usb controller you do not need anything extra to work with these examples. In addition you will find several for mss storage.

Best Regards,

Sabina

0 Kudos
Reply

3,057 Views
rajkumar_yerraj
Contributor II

Thanks alot for the information Sabina.

0 Kudos
Reply

3,057 Views
mjbcswitzerland
Specialist V

Hi

Full Speed USB has an internal transceiver but High Speed USB requires an external HS one.
See the free uTasker open source project for USB-MSD device to SD card, Flash, SPiIFlash (and composites) at links below, which include also K60 and USB simulation for simplest development and understanding.

Regards

Mark

Complete Kinetis solutions for faster/more efficient professional needs, training and support: http://www.utasker.com/kinetis.html
i.MX RT project compatibility: http://www.utasker.com/iMX.html
Including FreeRTOS integration for all Kinetis parts


Kinetis: http://www.utasker.com/kinetis.html
Kinetis K60:
- http://www.utasker.com/kinetis/TWR-K60N512.html
- http://www.utasker.com/kinetis/TWR-K60D100M.html
- http://www.utasker.com/kinetis/TWR-K60F120M.html
- http://www.utasker.com/kinetis/ELZET80_NET-KBED.html
- http://www.utasker.com/kinetis/ELZET80_NET-K60.html

uTasker: supporting >1'000 registered Kinetis users get products faster and cheaper to market

Request Free emergency remote desk-top consulting at http://www.utasker.com/services.html

Open Source version at https://github.com/uTasker/uTasker-Kinetis

https://community.nxp.com/thread/512558
https://community.nxp.com/thread/352862
https://community.nxp.com/thread/498809

0 Kudos
Reply