How to get SAI running with FRDM-KL28Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get SAI running with FRDM-KL28Z

871件の閲覧回数
christoffer
Contributor I

Hi,

Is there any example on how to get SAI running with FRDM-KL28Z using SDK_2.2_FRDM-KL28Z?

 

I have tried with the below code to send some bytes but it hangs in the SAI_WriteBlocking. This due to register bit FWF (Enabled transmit FIFO is empty) will not be set after sending first word. Anyone knows why?

Best regards,

Christoffer

////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

#define BUFFER_SIZE (64)

uint8_t srcBuff[BUFFER_SIZE];

sai_config_t  user_config;

 sai_transfer_format_t   user_format;

user_config.protocol = kSAI_BusPCMA,
user_config.masterSlave = kSAI_Master;
user_config.mclkSource = kSAI_MclkSourceSysclk;
user_config.bclkSource = kSAI_BclkSourceMclkDiv;
user_config.syncMode = kSAI_ModeAsync;

SAI_TxInit(I2S0, &user_config);

user_format.bitWidth = 16;
user_format.channel = 0;
user_format.masterClockHz = 24000000;
user_format.protocol = kSAI_BusPCMA;
user_format.sampleRate_Hz = 8000;
user_format.stereo = kSAI_Stereo;
user_format.watermark = 4;

SAI_TransferTxSetFormat(I2S0,&user_handle,&user_format,25000000,24000000);


SAI_TxEnable(I2S0,true);

SAI_WriteBlocking(I2S0, 0, 16, srcBuff, BUFFER_SIZE);

タグ(1)
0 件の賞賛
返信
1 返信

748件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi christoffer,

There are several SAI examples in SDK_2.2_TWR-KL28Z72M. Maybe you can refer these examples.

SAI in SDK_2.2_TWR-KL28Z72M.png

I try to test the SAI interrupt_transfer example in SDK_2.2_TWR-KL28Z72M with default sai_config.

Just modify the code shown below.

I can hear the tone from headphone which connect to J7-SGTL5000.

SAI interrupt_transfer SDK_2.2_TWR-KL28Z72M.png

Have you try to use other user_config.protocol, for example:

user_config.protocol = kSAI_BusLeftJustified;

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信