How to get MK51DX128CLH7 into MCUXpresso?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get MK51DX128CLH7 into MCUXpresso?

ソリューションへジャンプ
3,566件の閲覧回数
Bert2
Contributor II

Hi,

I'm trying to find out how to work with the MK51DX128CLH7 in Xpresso. I found the MK51DX256CLK10 in a SDK but not the 128.

Do I have to use the generic M4?

Thanks in advance,

regards,

Bert

0 件の賞賛
返信
1 解決策
3,552件の閲覧回数
ErichStyger
Specialist I

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

元の投稿で解決策を見る

4 返答(返信)
3,562件の閲覧回数
ErichStyger
Specialist I

If they share the same peripherals, but are only different by the flash size, you should be able to use the smaller part, but change the linker file for the larger memory size.

0 件の賞賛
返信
3,557件の閲覧回数
Bert2
Contributor II

Hi, thanks for your quick answer. Unfortunately the devices differ in pinout (case) and peripherals.

0 件の賞賛
返信
3,553件の閲覧回数
ErichStyger
Specialist I

Just an idea: KDS (Kinetis Design Studio) with Processor Expert supports that device:

ErichStyger_0-1647593299440.png

 

What I did for similar cases:

a) using the possibility to install Processor Expert in to MCUXpresso IDE (did that for earlier versions, have not checked if this is still possible with 11.5). see https://mcuoneclipse.com/2017/04/09/mcuxpresso-ide-installing-processor-expert-into-eclipse-neon/ how this would look like. Otherwise: I used KDS to generate everything and then used MCUXpresso (see b))

b) import/port the KDS project with Processor Expert. https://mcuoneclipse.com/2018/07/27/porting-processor-expert-projects-to-mcuxpresso-ide/

I know this is a bit challenging, but worked for me for several projects with devices which are not supported by the NXP MCUXpresso SDK.

I hope this helps,

Erich

 

3,546件の閲覧回数
Bert2
Contributor II

Thank you Erich,

that will probably be my way. I did not look into the older IDE because the website did redirect me to the newer one...

Thanks very much!

0 件の賞賛
返信