K32 L2A Force RESETn pin to be dedicated

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32 L2A Force RESETn pin to be dedicated

ソリューションへジャンプ
2,399件の閲覧回数
sachin_patel
Contributor IV

Hi,

 

I am using a Kinetis K32 L2A microcontroller in our design. As part of our model, we require the RESETn pin to be dedicated (i.e. it must not be possible from software to change it's pin mux state).

I can see in the Reference Manual Chapter 6.3.2: FTFA_FOPT[3]:

RESET_PIN_CFG: When set to 1, it says the following: "RESET_b pin is dedicated. The port is configured with pullup enabled, open drain, passive filter enabled".

Does this mean that the option to mux the pin as anything other than RESET_b is now disabled?

Thanks,

Sachin Patel

0 件の賞賛
返信
1 解決策
2,388件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,389件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @sachin_patel ,

Yes, if want to mux reset pin to other function, RESET_PIN_CFG must be zero.

 

Regards,

Jing

0 件の賞賛
返信