How to fix hardfault encountered when calling "thr joiner add" from shell

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to fix hardfault encountered when calling "thr joiner add" from shell

1,303 Views
davidandresky
Contributor II

I am working through the demo's in the Kinetis Thread Stack Demo Applications User's Guide. In section 10.5 I am encountering a hard fault every time I call "thr joiner add" from the shell interface. The sample project is "router_eligible_device" and I have tried this on two different FRDM-KW41Z boards.

0 Kudos
Reply
3 Replies

1,209 Views
davidandresky
Contributor II

Hi, I was using KDS but have since moved to MCUXpresso and associated SDK's. I have not returned to this example since switching IDE's so I don't if it is still an issue.

0 Kudos
Reply

1,209 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

The supported IDEs for the FRDM-KW41z are currently MCUXpresso and IAR.

I tried running the section 10.5, you will see a difference when you send the command thr joiner view

Documentation: 

$thr joiner view
Index EUI PSK
0 0xFFFFFFFFFFFFFFFF kinetis

Actual result: 

$thr joiner view
Index EUI PSK
0 0xFFFFFFFFFFFFFFFF THREAD

I attach some screenshots from the process I followed: 

1.PNG

REED (Node A)

2.PNG

ED (Node B) 

Best Regards, 

Estephania 

0 Kudos
Reply

1,209 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

Which IDE are you using ? 

Best Regards, 

Estephania 

0 Kudos
Reply