How to efficiently shift long bit-strings in kinetis?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to efficiently shift long bit-strings in kinetis?

1,353 Views
diegocolombo
Contributor IV

Hi

once i receive a serial code i have to put it in a variable from right to left or left to right.If the bit-string is shorter than 32 bit it is easy ,it should work even in this trivial way:

unsigned int rx_bit_var,final_var;


for(i=0;i<bit_str_lngth;i++)
{
rx_bit_var=RecvFuction();//i waste a int for a bit ,it can be 0x00000001 or 0x00000000 

final_var |=rx_bit_var;
final_var <<=1;
}‍‍‍‍‍‍‍‍‍‍

but what if the string is 100 bits long?
In a 9S08 i would dare to rotate variables through carry.
Is there any hardware in low end Kinetis microcontroller that can ease ths process?
It would be possible to profite of some register in serial modules as SPI,I2C or UART?
Many thanks

1 Reply

1,261 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Diego,

I think you can use the bits segment  variable in C language:

typedef union
{
    unsigned int word0,word1;
    struct Bit {
         unsigned int half_Ba0: 4;
         unsigned int half_Bb0: 4;
         unsigned int half_Bc0: 4;
         unsigned int half_Bd0: 4;
         unsigned int half_Ba1: 1;
         unsigned int half_Bb1: 2;
         unsigned int half_Bc1: 3;
         unsigned int half_Bd1: 4;
         unsigned int half_Ba2: 4;
         unsigned int half_Bb2: 4;
         unsigned int half_Bc2: 4;
         unsigned int half_Bd2: 4;
         unsigned int half_Ba3: 1;
         unsigned int half_Bb3: 2;
         unsigned int half_Bc3: 3;
         unsigned int half_Bd3: 4;
         } B;

}u_var;
 u_var word;

void main()

{

  word.word0=0x12345678;
  word.B.half_Bd1=0x07;

.........

}

I have tried above code, I can pass compilation with KDS tools.

Hope it can help you

BR

Xiangjun rong