How to display internal uP config registers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to display internal uP config registers

ソリューションへジャンプ
2,166件の閲覧回数
holyhope
Contributor III

Hi to all,

I'm developing on K60 with KDS 2.0.0

I want to see , when debugging, the uP config register like CFG1 of ADC0?

There is possibility to show Register like R1 ecc... that are internal register , i want only see the configuration register.

With PEx there is the page "Configuration Register" but it is an offline version, I want something that the debug ask to the board! So in this way I'm sure that the configuration register is the correct numbre present on this time on the board

what I can do?

thanks,

Max

0 件の賞賛
返信
1 解決策
1,962件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
1,963件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
1,962件の閲覧回数
holyhope
Contributor III

Many thanks for your answer.

Now I'm installing the plug in!!!

In the description is the perfect plug in for me!

The mcuoneclipse.com tell me another very important information!

thanks,

Massimiliano


Edit: I installed and test this plug-in.... All Works right! thanks,

Massimiliano

0 件の賞賛
返信