How to display internal uP config registers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to display internal uP config registers

Jump to solution
2,183 Views
holyhope
Contributor III

Hi to all,

I'm developing on K60 with KDS 2.0.0

I want to see , when debugging, the uP config register like CFG1 of ADC0?

There is possibility to show Register like R1 ecc... that are internal register , i want only see the configuration register.

With PEx there is the page "Configuration Register" but it is an offline version, I want something that the debug ask to the board! So in this way I'm sure that the configuration register is the correct numbre present on this time on the board

what I can do?

thanks,

Max

0 Kudos
Reply
1 Solution
1,979 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
1,980 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
1,979 Views
holyhope
Contributor III

Many thanks for your answer.

Now I'm installing the plug in!!!

In the description is the perfect plug in for me!

The mcuoneclipse.com tell me another very important information!

thanks,

Massimiliano


Edit: I installed and test this plug-in.... All Works right! thanks,

Massimiliano

0 Kudos
Reply