How to display internal uP config registers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to display internal uP config registers

跳至解决方案
1,498 次查看
holyhope
Contributor III

Hi to all,

I'm developing on K60 with KDS 2.0.0

I want to see , when debugging, the uP config register like CFG1 of ADC0?

There is possibility to show Register like R1 ecc... that are internal register , i want only see the configuration register.

With PEx there is the page "Configuration Register" but it is an offline version, I want something that the debug ask to the board! So in this way I'm sure that the configuration register is the correct numbre present on this time on the board

what I can do?

thanks,

Max

0 项奖励
回复
1 解答
1,294 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
2 回复数
1,295 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1,294 次查看
holyhope
Contributor III

Many thanks for your answer.

Now I'm installing the plug in!!!

In the description is the perfect plug in for me!

The mcuoneclipse.com tell me another very important information!

thanks,

Massimiliano


Edit: I installed and test this plug-in.... All Works right! thanks,

Massimiliano

0 项奖励
回复