How to create a real time GUI to interface with K60?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to create a real time GUI to interface with K60?

1,548 Views
broccolee
Contributor III

Hi,

I am using TWR-K60N512, with PK60DN512Z VMD10 chip. I'm using Codewarrior 10.5 for debugging and I'd like to create a GUI to interface with the K60 that will be controlling multiple stepper motors. I'd like to use the mouse and keyboard as inputs. Is this possible? If so, can someone provide a brief tutorial on how to do it and what kind of program I should be using to create the GUI? If not, are there other ways to do something similar?

Thanks.

0 Kudos
Reply
2 Replies

1,409 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Lim,

Can you use Freemaster tools to establish a GUI so that you can monitor the variables and control the application while the target board is running.

This is Freemaster tools website:

FreeMASTER Run-Time Debugging Tool|NXP

You can download and install the Freemaster tools on your PC, there are a lot of DOCs which introduces how to use Freemaster tools.

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

1,409 Views
broccolee
Contributor III

Thanks Rong. Will give this a try.

0 Kudos
Reply