How to create a real time GUI to interface with K60?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to create a real time GUI to interface with K60?

1,583件の閲覧回数
broccolee
Contributor III

Hi,

I am using TWR-K60N512, with PK60DN512Z VMD10 chip. I'm using Codewarrior 10.5 for debugging and I'd like to create a GUI to interface with the K60 that will be controlling multiple stepper motors. I'd like to use the mouse and keyboard as inputs. Is this possible? If so, can someone provide a brief tutorial on how to do it and what kind of program I should be using to create the GUI? If not, are there other ways to do something similar?

Thanks.

0 件の賞賛
返信
2 返答(返信)

1,444件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Lim,

Can you use Freemaster tools to establish a GUI so that you can monitor the variables and control the application while the target board is running.

This is Freemaster tools website:

FreeMASTER Run-Time Debugging Tool|NXP

You can download and install the Freemaster tools on your PC, there are a lot of DOCs which introduces how to use Freemaster tools.

Hope it can help you

BR

Xiangjun Rong

0 件の賞賛
返信

1,444件の閲覧回数
broccolee
Contributor III

Thanks Rong. Will give this a try.

0 件の賞賛
返信