How to change the logical output voltage of FRDMKW36?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to change the logical output voltage of FRDMKW36?

ソリューションへジャンプ
1,350件の閲覧回数
Enjoy
Contributor II

Hi there:

I want to drive a external ADC by FRDMKW36, while when I set one GPIO of MKW36 to 1, the output voltage is only about 1.8v and too low to enable the ADC. So can the logical output volatage of GPIO rise to about 3v in FRDMKW36?

May somebody help me?

Thanks.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,343件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please check this Application Note: DC-DC Power Management?

The FRDM-KW36 can be configured to use any of the DCDC converter operating modes. The board is configured in Buck (Auto-Start) by default.

Also, please refer to FRDM-KW36 Freedom Development Board User's Guide. (Section 3.3: Power management).

Hope this helps.

 

Regards,

Ricardo

Best Regards,
Ricardo

元の投稿で解決策を見る

2 返答(返信)
1,344件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. Could you please check this Application Note: DC-DC Power Management?

The FRDM-KW36 can be configured to use any of the DCDC converter operating modes. The board is configured in Buck (Auto-Start) by default.

Also, please refer to FRDM-KW36 Freedom Development Board User's Guide. (Section 3.3: Power management).

Hope this helps.

 

Regards,

Ricardo

Best Regards,
Ricardo
1,339件の閲覧回数
Enjoy
Contributor II
Thank you so much and the problem has been solved.
0 件の賞賛
返信